Hi All,
I'm using DM816X custom board in my project.
Using ADV7182 decoder for CVBS IN.
When I use dm816x_hdvpss.xem3 firmware which is used in DM816X EVM board to load VPSS, I'm getting log like below, and fails to load firmware.
FIRMWARE: Ipc_CONTROLCMD_STARTCALLBACK Error: ProcMgr status 0xffffffff FIRMWARE: Could not start: -1
notify_send_event failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
But when I use ti816x_hdvpss.xem3 firmware file in custom board, firmware loads successfully.
When I try to load ti816x_hdvpss.xem3 firmware in DM816X EVM board, I'm getting same above prints in console.
What is the difference between these two firmwares.
Whether from board to board firmware will differ?
In VPSS firmware code any ADV7182 decoder specific configurations to be taken care.
Is there any firmware binary which can be used in EVM board as well as in custom board.
Can any one please help me to solve this issue.
Thanks and Regards,
NIthin