Hi,
I have a question about SYSBIOS.
I'm using C6670 with SYSBIOS and want to lower the power consumption.
The TSK threads of SYSBIOS are running on each core of C6670(4 cores).
Can power consumption be lowered by controlling operation of TSK thread well?
For example, usually put the TSK of each core in IDLE state and make TSK to run only when required.
Or if SYSBIOS are running, does TSK state effect to the power consumption?
best regards,
g.f.