Hi,
We are using 1.25GHz IND Version 6678 for Prototyping. I have used the Power Spreadsheet to calculate the Current requirement . I have attached the same. In spreadsheet ,the CVDD voltage is fixed at 0.85V. But it is a variable voltage from 0.7 to 1.1V through VID interface. How to set the CVDD at 1.1V in spreasheet
Also,I found the difference in the current specification for 1.25GHZ processor between the attached spreadsheet and following TI Link :http://www.ti.com/analog/docs/refdesignovw.tsp?familyId=64&contentType=2&genContentId=149652#sysmonsup.
The TI link says CVDD requirement is 12.9A for 1.25GHz@85'C.
Please confirm which one i should consider for selecting Power driver.
Regards,
Sakthi.A
4643.5468.C6678_Power_Consumption_Summary_Rev3_4.pdf