I was reading through the datasheet on the TMS320C6747 DSP and noticed the power-off sequence information was sparse at best. It states:
"6.3.2 Power-off Sequence
The power supplies can be powered-off in any order as long as the 3.3V supplies do not remain powered
with the other supplies unpowered."
What it doesn't state is any information about the severity and consequences of small overlaps in the 1.2V and 3.3V power-off sequencing. Is a small period of time of 3.3V remaining powered when the 1.2V falls out of spec OK as long as it doesn't happen often?
Also, there doesn't seem to be any mention of how low the 3.3V rail has to be to assure it is 'off' during power-off sequencing? Does anyone have experience with what this value would be? 3V? 2.7V? 2V?
Thanks.