Hello,
I have the following problem with the c6678EVM:
I have connected the card to my PC using TMDXEVMPCI, but the device does not show up with lspci on Linux, neither Windows finds it. In this PC I have a Gigabyte Z8-HD3 motherboard. When I connect the same board with the same settings to an other PC with a different motherboard it is listed by lspci and I can see that the PCIe registers are configured after boot.
I have tried both PCIe slots (a 4x and an 16x one) with the Z8-HD3 motherboard but none of them works: the card boots, I can access it via the USB cable, but it is not recognized by lspci.
Do you know of any compatibility issues with this type of motherboard?
What do you suggest, how do I proceed with this problem?
Thank you,
Peter