This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what is the statement to toggle an output pin with 3.3v?



What is the statement to toggle an output pin with 3.3v (the gpio of an STM32w 108cc)? I want to add a statement to the program written that indicate that the output of the gpio of the stm32 is 3.3v.pleaaaaaaaaaase I need help

p { margin-bottom: 0.25cm; line-height: 120%; }

#include "contiki.h"
#include "dev/button-sensor.h"
#include "dev/leds.h"
#include "dev/gpios.h"
#include <stdio.h>
#include "board.h"


/*---------------------------------------------------------------------------*/
PROCESS(test_button_process, "Test button");
AUTOSTART_PROCESSES(&test_button_process);
/*---------------------------------------------------------------------------*/
PROCESS_THREAD(test_button_process, ev, data)
{
   
PROCESS_BEGIN();

   
SENSORS_ACTIVATE(button_sensor);
   
boardPrintStringDescription();
   
printf("Press the button to toggle the leds.");
  
   
while(1) 
   
{
      
PROCESS_WAIT_EVENT_UNTIL(ev == sensors_event && data == &button_sensor);
      
leds_toggle(LEDS_ALL);
      
gpios_toggle(GPIOS_RELAY);

        I want to add the statement here that indicate  the output of the pin (the gpio of the stm32w108cc)
   
}
  
   
PROCESS_END();
}
/*---------------------------------------------------------------------------*/