Other Parts Discussed in Thread: TMS320C6743
Hi,
I'm involved in SW development for custom board based on TMS320C6743 DSP. The board has SDRAM, NAND FLASH, 2 UARTs and CODEC connected to DSP. I plan to use SYS/BIOS and CCS v5. And I have no expeirence on TMS320C67x. Also there are no working examples on this architecture before me.
The simple project created from the CCS v5 wizard for TMS320C6743 and SYS/BIOS doesn't work on the board. XDC560v2 USB is connected to the processor. The program is loaded but doesn't reach main(). When I switch full check on for program loading the program loading is failed.
At first sight there are no C6743-specific GEL, CSL and examples. There are examples for С6747/8 and OMAPL137.
I will be very appreciated for any advices how to start developing for stand alone C6743 and where I can find C6743-specific information!