It seems the C672x Chip Support Libraries don't compile with Code Composer Studio 4.
When I try to compile the spi_example project I get the following linker error:
undefined symbol: int00
error: unresolved symbols remain
warning: entry-point symbol "int00" undefined
warning: no suitable entry-point found; setting to 0
Can anyone help?
Thank you very much in advance,
GergelyB