1. Where can download TMS320C5532 reference schematic?
2. How to burn the code to TMS320C5532, can use USB??we have no enough UART & SPI to use.
3. TMS320C5532 can support Ambarella A12/S2L? where can download the driver?
thx!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. Where can download TMS320C5532 reference schematic?
2. How to burn the code to TMS320C5532, can use USB??we have no enough UART & SPI to use.
3. TMS320C5532 can support Ambarella A12/S2L? where can download the driver?
thx!
Hi,
Any particular reason for selecting TMS320C5532 V/s TMS320C5535 ?
Below is response for your questions:
A1. I do not think we have a reference schematic specifically for C5532 but there exists C5535 eZDSP reference schematic. But the features that are not supported by C5532 such as LDOs (DSP & USB LDO) etc needs to be accordingly taken care.
C5535 ezDSP - reference link - support.spectrumdigital.com/.../
A2. As mentioned in the datasheet high-speed Universal Serial Bus (USB 2.0) is not available on TMS320C5532. This feature is not supported in C5532 not sure about your exact requirements to further suggest.
A3. Could you provide additional details on this.
Hope this helps.
Regards
Vasanth