Hi,
Another question :
Is it possible (I am sure it is...) to connect an ads8327 ADC to one of the C6748's SPI Port ?
I my application I will need the ADC to work in AUTO TRIGGER mode.
As far as Pin connexion is concerned, here is what I've understood :
(ADC) SDO connect to : (DSP) MISO
(ADC) SDI connects to : (DSP) MOSI
(ADC) SCLK connects to : (DSP) SCLK
(ADC) CS/FS connects to : (DSP) /SCS[n]
I'm not sure I'm right for these signals above but I defenitele do not know what to do with these three other signals :
(ADC) /CONVST
(ADC) EOC
(ADC) INT