I need to verify the differences, if any, of the "C", "D", and "E" variants of the C6414 and C6415 devices.
The silicon errata sprz011t.pdf, page 9, indicates that "C" is rev 1.03, "D" is 1.1, and "E" is 2.0.
However, I have devices labelled "C20" and "D20", which according to the same page, are Silicon Rev 2.0 devices. The internal memory of the device confirms that they are rev 2.0.
So, what do the "C", "D", and "E" identifiers refer to?