board not communicate with UART.what I do ?In windows which file we want generate, linux which file we want to generate suppose kit will be bootable what data we will get from the hardware.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
board not communicate with UART.what I do ?In windows which file we want generate, linux which file we want to generate suppose kit will be bootable what data we will get from the hardware.
hi ,
can u tell me these two steps how to do?
how to gmake is present inside xdc package. xdc path is already in same folder
Build is done by executing gmake. “gmake” is present inside XDC package. For “gmake” to be available in windows command prompt, the XDC path must be set in the windows system path.
IMPORTANT NOTE: xdc path is needed to be set in environment variables.
If not, then set it using the set PATH =
<Install_dir>/ti_components/os_tools/windows/xdctools_x_xx_xx_xx;%PATH
% in command prompt
Hi Kalaiventhan,
Have you installed the Linaro gcc toolchain? It seems that this is missing.
Regards,
Rishabh
when run gmake.exe using command window after complete I got this kind of message.
Kalaiventhan,
Once you have downloaded and installed the GCC compiler from to a folder like C:\ti\gcc-arm-none-eabi-4_9-2015q3
In Tools_path.mk, you would need to change the following line
CODEGEN_PATH_A15 ?=$(TI_SW_ROOT)/cg_tools/linux/gcc-arm-none-eabi-4_9-2015q3
to
CODEGEN_PATH_A15 ?=C:\ti\gcc-arm-none-eabi-4_9-2015q3
Regards,
Piyali
Hi,
You need to set CODEGEN_PATH_EVE value in tools_path.mk for this.
Regards,
Rishabh
my path chaged like this
ifeq ($(BUILD_OS),Windows_NT)
CODEGEN_PATH_DSP ?= C:\VISION_SDK_02_12_00_00\ti_components\cg_tools\windows\C6000_7.4.2
CODEGEN_PATH_EVE ?= C:\VISION_SDK_02_12_00_00\ti_components\cg_tools\windows\arp32_1.0.7
CODEGEN_PATH_A15 ?= C:\VISION_SDK_02_12_00_00\ti_components\cg_tools\windows\4.9 2015q3
CODEGEN_PATH_M4 ?= C:\VISION_SDK_02_12_00_00\ti_components\cg_tools\windows\ti-cgt-arm_5.2.5
endif
how to change this below line,these are in makefile fist
ifeq ($(BUILD_OS),Windows_NT)
TI_SW_ROOT := $(abspath ..)/ti_components
endif
I have installed XDC tools...also I attached my tools path file .my error also I attached below
Hi,
Can we have a webex. You still have not set the correct value for A15 tool chain path.
Regards,
Rishabh
Hi Rishabh,
We have the below list of files generated under the directory
"C:\VISION_SDK_02_12_00_00\vision_sdk\binaries\tda2xx_evm_bios_all\vision_sdk\bin\tda2xx-evm"
1. As per the Manual, "vision_sdk_a15_0_debug.xa15fg" needs to be generated, but we have "vision_sdk_a15_0_release.xa15fg" generated.
Please advice either debug/release is fine.
2. Also, we do not have the below files in the path.
a. "vision_sdk_arp32_4_release.xearp32F".
b. "vision_sdk_arp32_3_release.xearp32F".
We are not able to load the above binaries.
How the above files can be generated, or any idea why the files are not generated.
Thank you.
ok thanks..We are connected LCD like this image, strip connection possible like what we are connected. But board indication is 1 and 1,we are not connected based on mark indication,it is correct ?