Other Parts Discussed in Thread: SYSBIOS, TM4C1294NCPDT
Tool/software: TI-RTOS
I am unable to enable runtime instance in BIOS which is essential for creating tasks or semaphores dynamically
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI-RTOS
I am unable to enable runtime instance in BIOS which is essential for creating tasks or semaphores dynamically
I am2350.Dynamic TAsks_SWI_empty_EK_TM4C1294XL_TI_Blink.rarusing latest version of TI RTOS and CCS .. I adapted from the example projects given for TI RTOS (lab 8) optional.
7077.TAsks_SWI_empty_EK_TM4C1294XL_TI_Blink.rarI rebuilt a new veriosn of the project but issues remian.
Attaching.
I am using the latest version of RTOS and CCs, All SW is up to date.
Unable to create Runtime instance for semaphore. Heap also not getting set. I tried with cfg script and with GUI. It does not work. I have bundled the project with a previous mail thread for your perusal.
Thank you
Attaching the project once again.
Unable to create run time instance for Optional la8 of TI RTOS Workshop. I tried GUI as well as text --manual addition of CFG . It does not work.
These are the build errors"
**** Build of configuration Debug for project TAsks_SWI_empty_EK_TM4C1294XL_TI_Blink ****
"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 8 all -O
making ../src/sysbios/sysbios.aem4f ...
gmake[1]: Nothing to be done for 'all'.
'Building file: ../empty.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.12.0.STS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/Users/pramanujam/workspace_v7/TAsks_SWI_empty_EK_TM4C1294XL_TI_Blink" --include_path="C:/Users/pramanujam/workspace_v7/TAsks_SWI_empty_EK_TM4C1294XL_TI_Blink" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.12.0.STS/include" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE -g --gcc --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="empty.d" --cmd_file="configPkg/compiler.opt" "../empty.c"
>> Compilation failure
subdir_rules.mk:16: recipe for target 'empty.obj' failed
"../empty.c", line 103: error #148: declaration is incompatible with "const ti_sysbios_knl_Semaphore_Handle LEDSem" (declared at line 11 of "C:/Users/pramanujam/workspace_v7/TAsks_SWI_empty_EK_TM4C1294XL_TI_Blink/Debug/configPkg/package/cfg/empty_pem4f.h")
1 error detected in the compilation of "../empty.c".
gmake: *** [empty.obj] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
After this build failure cfg file shows runtime enabled and heap size 4096.
Regards