Part Number: TMDSLCDK6748
Other Parts Discussed in Thread: THS1206
Dear Sir,
Sir i am trying ADC configuration with LCDK6748 today again with the EMIF method as from start i was working on it. I have verified the TEST MODE of ths1206 and its respond over changing the register value as per given in table, & its functioning as specified with out any modification in design as we have made earlier. But sometimes we need to change the JUMPER connections at W1 & W11 so that we can adjust get change over in internal voltage and external voltage that is like switching Vref mode.
As per instructions given in THS1206 interface example(slaa094_R1slaa094_r1.pdfsprufl6f_R1.pdf.pdf) - and shown in figure no. 25 here CSO which is initially active low after that it will goes high and at time of dat available (/RD=1) it again goes to high but after that it is not getting active low please brief us how to get control over it.[ PAGE NO 23,SLAA094.pdf]
Second thing is that as mentioned in TABLE 2 EMIFA pins specific to SDRAM ( spruf6f_R1.pdf,pg.no 13) EMA_CS0 please brief us regarding the same as it is also not functioning the same way as mentioned .