Trying to reproduce the set up in the following TI Design
http://www.ti.com/tool/tidep0061
Downloaded the software zip file which consists of the following 8 files
Archive: sorte-tidcd07.zip
Length Date Time Name
-------- ---- ---- ----
0 12-09-16 17:15 Software/
0 12-09-16 17:15 Software/device/
11202 12-08-16 11:24 Software/device/appl_slave.asm
0 12-09-16 17:16 Software/master/
5829 12-09-16 17:16 Software/master/app_cnc_macros.inc
14057 12-09-16 17:16 Software/master/cnc_app.asm
13027 09-12-16 08:26 Software/TIDEP0061SimpleOpenReal-TimeEtherne_manifest.html
13487 09-07-16 09:54 Important Notice for TI Designs.pdf
-------- -------
57602 8 files
however, the .inc file includes other files that are not part of zip file and it is not obvious what other software packages I may need. Can someone point me in the right directions with regards to what additional software package needs to be installed prior to zip file above. It would be great if this was added to TI Design doc or downloadable zip file.
Thank you in advance!