Tool/software: Linux
i have a custom board based on am437x-evm,i try using am437x-evm-gb.dtb file and zImage,i could get in kernel and rootfs without modify the kernel sourec file(from ti-sdk).but when i try to control the gpio pin on my board by /sys/class/gpio/ direction,i failed to do that without any error or waring,the gpio pin value still no change after i do sth,but i do the samething on the custom board kernel and dtb file given by the custom board manufacturer, i can success change the pin value.so i doublt the difference between my board and am437x-evm borad,so i try replacing am437x-evm-gp.dtb by my custom board dtb file,but the result as below
it hang out here Staring kernel
then i replaced am347x-evm-gp(zImage) by my board offical uImage file,as bellow
it's hang out here too,
why could cause these appearance?it's unbelievable to me......