I have a question about the UART on AM3517.
The AM3517 TRM says the UART is compatible with 16C750.
1) Is it possible to connect to OMA3530 with AM3517 directory via the UART I/F ?
2) The UART of LM3S3749(Stellaris) has similar functionality with 16C550, so is it also possible to connect to LM3S3749 with AM3517 via the UART I/F
3) The LM3S2B93(Stellaris) Data sheet describes the UART of LM3S2B93 has similar functionality with 16C550, so is it also possible to connect to LM3S2B93 with AM3517 via the UART I/F ?
Thanks and Best Regards,
KIMIZUKA