Tool/software: Linux
Hi,
I would like to ask about the performance of USB on omapl137 platform. Reading the LSP 02.20 Linux Drivers Datasheet, I see that the max speed attained on CDC devices can be (table on pg 24) 36Mbps . Can i ask why is it so low? USB high-speed should give us a throughput of 480Mbps or so?
Thanks,
AQ