Hi
I have two main queries listed below:
1. Is it necessary to stick with the AS length and skew requirements given in datasheet Table 8-75? Is it ok if we length exceeds to 200mils, then the required 100 mils.
2. Is there any constraint that clock should be lengthier than all other address and control signals? Similarly, is there any constraint if DQS should be lengthier than DQ signals?
Thanks and Regards
SUSHRUTA