Other Parts Discussed in Thread: OMAP-L137,
Tool/software: Code Composer Studio
Hello.
In the datasheet for the OMAP-L137 figure 6-12 it clearly shows a flash connected to the processor's EMIFA using the open NAND flash interface (ONFI).
I am using the high-temperature version of this processor: OMAPL137-HT. Nowhere in the OMAPL137-HT datasheet is there any mention on ONFI support.
My question is: does the OMAPL137-HT also support ONFI?
And more generally, if I see something is supported by the OMAP-L137 is it safe to assume it is also supported by the OMAPL137-HT?
Thanks in advance,
Alejandro