Other Parts Discussed in Thread: TIDA-00455
Hi!
TIDA-00455 is designed to capture 4 HD streams (through FPDLink and OV490) on two ports of one slice of VIP on TDA.
Each port(PortA/PortB) of a VIP slice is capturing data in multiplexing mode.
According to TDA2x TRM(as I understand it) this scenario is not available.
Table 9-13 in chapter <9.4.5.8.1 Multiplexing Scenarios> shows:
Maximum Channels in Dual 8- Inerface Clock Rate(MHz)
bit Data Interface Mode -
Interleaved Channels per
Single 8-bit Port.
One 16-bit VIP can be
configured to support two such
8-bit ports.
HD Progressive n/a 148.5
Can somebody explain me, is my understanding wrong or is it a conflict? Is it possible to capture 2 multiplexed HD streams on one 8-bit port in TDA2x?
Thank you.