Other Parts Discussed in Thread: AM3359, TPIC2810, PCA9536, SN65HVS882, TPS65910
Tool/software: Linux
Dear ,
I have booted the ICEv2 board through SD Card but it does not show any ethernet device when I gave ifconfig command and link is placed at ICSS location not CPSW position.
But if I place the link at CPSW position and again booted the ICEv2 board it shows eth0 and eth1 devices.
I want to see these two devices eth0 and eth1 in ICSS link postion which is not happening.
SD Card is of 8 GB and having these files:
1>am335x-icev2.dtb
2>arago-base-tisdk-image-am335x-evm.tar.xz
3>MLO
4>u-boot.img
5>zImage
Please let me know what is problem with the setup or any mistake.
Thanks in advance.
Ashok Wakode