Other Parts Discussed in Thread: OMAPL138, DA8XX
Tool/software: Linux
I am working with a custom OMAP L-138 based board that is similar to the LCDK. Our board uses UART0 for the console, the LCDK uses UART2. I am trying to modify the existing LCDK code to use UART0. The changes I have made so far allow U-Boot to use UART0, but after Linux is copied into memory and I get the message "Starting Linux ...", I don't get any more console output from Linux. Using the JTAG debugger, I can see that Linux is loading into memory and running, just no console output.
- I'm using MCSDK 1.01.00.
- I modified omapl138_lcdk.h and omapl138_lcdk.c to get U-Boot working on UART0
- I modified the CONFIG_BOOTARGS definition changing console=ttyS2 to console=ttyS0 assuming Linux would use UART0 for the console after the change, but it didn't work.
Please advise me on the proper method of changing the UART in Linux. Thanks.