Tool/software: Linux
Hi, all
My platform is DM8127, rdk is rdk3.8.0.
When I configure the sensor output bt1120 data to dm8127.
where i need to configure to tell the data is bt1120?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi, all
My platform is DM8127, rdk is rdk3.8.0.
When I configure the sensor output bt1120 data to dm8127.
where i need to configure to tell the data is bt1120?
Hello,
As far as I know, DM81x ISP doesn't support BT.1120 (though it supports BT656). At least this is not covered in the TI TRM !
Ideal place to configure such information is ISP/ISIF. You can have a look at ISIF_CCDCFG.
You may have to add a TVP5x decoder on to your device !
Hi,Ravikiran
Thanks for your answer.
We use soc sensor to output 16bit yuv data.
I saw the datasheet: Parallel Connection for Raw (up to 16-Bit) and BT.656 or BT.1120 (8- and 16-Bit) .
If i configure ISIF_REC656IF and ISIF_CCDCFG ,then it can capture the right image?
Tim, Regards.