Part Number: DRA797
Does the J6Entry's DCAN IP conform to ISO 16845-1:2016 [Conformance Test Plan link Layer / PHY]?
From https://www.iso.org, the "ISO 16845-1:2016 specified the conformance test plan for the CAN data link layer and the physical signaling as standardized in ISO 11898-1. This includes the Classical CAN protocols as well as the CAN FD protocols".
I believe that the Jacinto6 family of devices licenses the Bosch IP; this may be a hint to conformance to ISO 16845-1:2016, but I can not confirm.
I checked the latest J6Entry Technical Reference Manual and found no reference to ISO 16845.
I checked the latest TI Android Test Plan for 6AM.1.3d and found no reference to ISO 16845 (as I suspected as this is too high level for data link layer and physical signaling...).
Can anyone in the community confirm this?