Hi all
I used the PSP2.0.0000 to compile cmemk and dsplink
cmemk is fine,but dsplink is wrong, the error is :
[root@OMAP3EVM /omap3530]# insmod dsplinkk.ko
insmod: cannot insert 'dsplinkk.ko': invalid module format
and I typed ----strings dsplink.ko | gre vernagic, it shows
vermagic=2.6.260omap1 mod_unload modversion ARMV7
-mod_vermagic6
-mod_vermagic6
but I check the cmemk.ko ,it is that:
vermagic=2.6.260omap1 mod_unload modversion ARMV7
-mod_vermagic5
-mod_vermagic5
I comile the dsplink throng the webpage :http://wiki.davincidsp.com/index.php/Building_DSPLink
step is
1 export DSPLINK and PATH ($DSPLINK/etc/host/script/linux)
2 edit BASE_BUILDOS and BASE_CGTOOLS in " make/Linux/omap3530_2.6.mk" and BASE_SABIOS and BASE_CGTOOLS in " $DSPLINK/make/DspBios/c64xxp_5.xx_linux.mk"
3 used perl dsplinkcfg.pl --platform=omap3530 --nodsp=1 --dspcfg_0=OMAP3530SHMEM --dspos_0=DSPBIOS5XX --gpp0s=OMAPLSP --comps=ponslrmc --trace= --legacy=1
4 use xdc -P clean and .interface command to dsp/src and gpp/src
5 make -s debug for them
where am I wrong ?
thanks for all