Hello,
I've posted few issues here but I've not heard anything back yet. What is the estimated response time?
https://e2e.ti.com/support/dsp/c5000/f/109/p/637967/2375550#2375550
Question#1: How do I convert the TIesr_C55_demo for C5535 to use SPI1 from the P2, Expansion Connector instead of using SPI2 or SPI0?
Question#2: I am having an issue with building a new trigger words under Ubuntu that I posted in the above link or here is the error that I get? What should I do for this error?
/usr/bin/ld: cannot find -lTIesrFA_ALSA
collect2: error: ld returned 1 exit status
nbproject/Makefile-LinuxDebugGnu.mk:57: recipe for target '../../Dist/LinuxDebugGnu/bin/testtiesrfa' failed
make[3]: *** [../../Dist/LinuxDebugGnu/bin/testtiesrfa] Error 1
make[3]: Leaving directory '/home/farzin/Desktop/TI/TIesr/c5535/TIesr_model_build/TIesrFA/TestTIesrFA'
nbproject/Makefile-LinuxDebugGnu.mk:54: recipe for target '.build-conf' failed
make[2]: *** [.build-conf] Error 2
make[2]: Leaving directory '/home/farzin/Desktop/TI/TIesr/c5535/TIesr_model_build/TIesrFA/TestTIesrFA'
nbproject/Makefile-impl.mk:39: recipe for target '.build-impl' failed
make[1]: *** [.build-impl] Error 2
make[1]: Leaving directory '/home/farzin/Desktop/TI/TIesr/c5535/TIesr_model_build/TIesrFA/TestTIesrFA'
Makefile:126: recipe for target 'TestTIesrFA' failed
make: *** [TestTIesrFA] Error 2
Thank you.