Part Number: TMDSCSK8127
Hi, I'm new to TMDSCSK8127.
The start kit (or sd card) seems to have a problem.
I followed the enclosed Quick Start Guide but I saw the "CCC...." in teraterm.
Saw a related post and tried to resolve the issue with no success.
The sd card that came with the kit did not include the demo binaries. I attempted to go through the procedure documented to setup the sd card. Ran into an issue running the mksd-t81xx.sh script.
sudo ./mksd-ti81xx.sh /dev/sdb ../../Source/ipnc_rdk/
[sudo] password for steve:
All data on /dev/sdb now will be destroyed! Continue? [y/n]
y
[Partitioning /dev/sdb...]
unmounting device '/dev/sdb1'
1024+0 records in
1024+0 records out
1048576 bytes (1.0 MB, 1.0 MiB) copied, 0.000953206 s, 1.1 GB/s
DISK SIZE - 1048576 bytes
CYLINDERS - 0
sfdisk: invalid option -- 'D'
Usage:
sfdisk [options] <dev> [[-N] <part>]
sfdisk [options] <command>
/dev/sdb1 * 2048 2056 9 4.5K c W95 FAT32 (LBA)
/dev/sdb2 10 2047 2038 1019K 83 Linux
Partition table entries are not in disk order.
The partition table has been altered.
Calling ioctl() to re-read partition table.
Syncing disks.
[Making filesystems...]
[Copying files...]
cp: error writing '/mnt/uImage': No space left on device