Using 480p/i resolution, is it possible to drive both outputs on the dm365? Thoughts?
Regards,
-Craig
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Using 480p/i resolution, is it possible to drive both outputs on the dm365? Thoughts?
Regards,
-Craig
CraigSmith said:Using 480p/i resolution, is it possible to drive both outputs on the dm365? Thoughts?
If you mean simultaneously than no, the DM365 has only three video DACs and in the component output case all three would be used leaving none for the composite. If you want to be driving component and composite simultaneously you would need some external hardware (i.e. an external video encoder).
If you mean to be able to switch between them than that is certainly possible.