Part Number: TMDSCSK8127
Tool/software: Code Composer Studio
Can someone explain the procedure for connecting to the DSP using the on-board USB emulator provided with the DM812CSK?
Using CCS version 5.5
CCS Target platform configuration: Connection=XDS100v2 USB, Board=DM8148
I can successfully connect to ARM CortexA8 (no gel file used loaded). When I try connecting to the DSP, the following error dialog pops-up:
Error connecting to the target:
(Error -6311) PRSC module failed to write to a register.
(Emulation package 6.0.14.5)
Thanks,
Jim