This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6742: C6742 programmer issue for mass production

Part Number: TMS320C6742
Other Parts Discussed in Thread: OMAP-L138

Hi all,

I provide the *.bin file to programmer factory for pre-programmer on NAND flash. Then forward NAND flash to SMT.

How to generate the *.bin :

1. CCS compile to generate *.out

2. AISgen convert *.out to *.bin ---> provide this *.bin to programmer factory 

Why this *.bin could not bring up by above procedure? But use sfh_OMAP-L138.exe to program this *.bin to NAND flash via UART that is ok.

May I know what conditions need to apply to programmer to resolve this issue?

E.g. programmer need to shift one block to do flash etc...

Thanks in advance.

B.R.

OC