Other Parts Discussed in Thread: TIDEP0076,
Tool/software: Linux
Hi TI experts
I'm trying to deploy TIDEP0076 design on AM5728, the target is to Generate point cloud with IDS ethernet based camera.
Recommended approaches in tiduc48b are:
1. use pre-build binaries
2. rebuild TIDEP0076 with bitbake by rebuiding SDK based on instruction processors.wiki.ti.com/.../Processor_SDK_Building_The_SDK
Option 1 is just for quick verification while option 2 is quite slow(maybe because of the great wall in China) and I haven't succeed.
I tried another approach: use installed TI SDK together with cmake to build TIDEP0076 based on dlp-sdk-2.0.tar.gz.
The options in cmake:
compiler is directed to ${TISDK}/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-gcc / g++
OpenCV install folder is directed to ${TISDK}/targetNFS/usr/share/OpenCV
Makefile is successfully generated.
While building the DLP sdk, I got error information below.
Strangely, I can't find where this clc.h is referred in this DLP sdk. This error is popped up during building opencl part.
For other part src like common folder, I can successfully build if I manually remove the opencl dependency.
Could you please help?
<built-in>:335:10: fatal error: 'clc.h' file not found
Makefile:9: recipe for target 'dlp_kernels.dsp_h' failed
make[3]: *** [dlp_kernels.dsp_h] Error 255
CMakeFiles/DLP_SDK_OPENCL.dir/build.make:57: recipe for target 'CMakeFiles/DLP_SDK_OPENCL' failed
make[2]: *** [CMakeFiles/DLP_SDK_OPENCL] Error 2
CMakeFiles/Makefile2:284: recipe for target 'CMakeFiles/DLP_SDK_OPENCL.dir/all' failed
make[1]: *** [CMakeFiles/DLP_SDK_OPENCL.dir/all] Error 2
Makefile:83: recipe for target 'all' failed
make: *** [all] Error 2