Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
hi,
We are using the TMS320 c6472 multicore dsp and we're experiencing unexplained behavior.
Our boot sequence is comprised of a secondary bootloader that configures the emac ant the local timers, afterwards it receives the actual image via the emac.
The image itself is built with sysbios 6.22, csl and our code.
The weird behavior is that 72 minutes after image loading the core experience shutdown (or at least the task stop running).
The secondary bootloader configures the local timers to be in dual unchained mode without the watchdog feature on.
Moreover it seems like it happens individually per core, e.g if core 2 loads 10 minutes after core 1 then the shutdown will be exactly 10 minutes after the shutdown of core 1.
When we print the "mode", "hi period" and "lo period" of the 6 local timers we see the secondary bootloader configuration on the cores without the image loaded, and the period was changed to the core with the image loaded but the mode stays the same.
We suspect bois_start changes the local times of the core but the new mode isn't wachdog mode either.
Can you help us figure out the reason of this shutdown?
regards,
eli