Other Parts Discussed in Thread: TPS53313, LM10011, TPS54424,
I'm looking at various different Power Supply options for the C6657 implementation. I've been told that the Smart Reflex feature is not optional for the Keystone I device. With that said, I've taken a look at the TPS53313 as the DC/DC converter option with an overall small package size. It looks to meet the voltage requirements and features a 0.6V reference.
Is this device a viable option to supply the 0.7V-1.1V of the C6655 when paired with the LM10011?