Tool/software: Code Composer Studio
Imported a legacy CCS 3.3 project into CCS 7.2. It is a custom board.
It used to build under CCS3.3
IN CCS 7.3 it complains about memory overflow. need help!
"SyncDMA.obj" "Time01.obj"
<Linking>
"C:/Users/HDL64-S3/dual-return/HDL2_Vaa_hallfailtest/EpromBoot11-02.cmd", line 34: error #10099-D:
placement fails for object ".text", size 0x3a60 (page 0). Available ranges:
RAM size: 0x4a00 unused: 0x2cdc max hole: 0x2cdc
error #10010: errors encountered during linking;
The memory allocation follows:
MEMORY
{
BOOT : origin = 0x0000, len=0x400,fill=0x0000
VECTOR : origin = 0x400, len=0x200
DATA : origin = 0x5100, len = 0x1000, FILL= 0X0000
MDATA : origin = 0x6100, len = 0x1B00, FILL = 0x0
DATA2 : origin = 0x7C00, len = 0x400, FILL= 0X0000
SECTIONS
{
.boot > BOOT
.vectors > VECTOR
.main: load= 0X600
.text >RAM
.bss >DATA
.data >DATA
.pend >RAM
.data2 >DATA2
.stack >RAM
.cinit >RAM
.far >RAM
}