Tool/software: Code Composer Studio
Hi
I have a full array microphone projects that use tmsc6748 、2 aic3106 and 4 microphones .
The structure diagram is shown below:
Every two microphones are connected to 3106,The i2s data is passed through axr12 and axr14 to tmsc6748. The both 3106 work fine.
C6748 prvide mclk、bclk and frame clock to 2 codecs.I use EDMA to receive data on the bus.
If I active one 3106 ,6748 can receive data from microphone.But when I activate two devices at the same time, C6748 can no longer receive any interrupt.
How do I configure two i2s signals that are connected to the McAsp bus properly?