Other Parts Discussed in Thread: OMAP-L137, OMAP-L138, MATHLIB
Team,
C674x/OMAP-L13x is now supported in the processor SDK:
http://software-dl.ti.com/processor-sdk-rtos/esd/OMAPL138/latest/index_FDS.html
The support per device, per platform and per board is documented in the different tables at:
http://software-dl.ti.com/processor-sdk-rtos/esd/docs/04_03_00_05/rtos/Release_Specific.html#supported-platforms
Now some questions:
1) The "DSP optimized lib" section does not list OMAP-L13x/C674x:
http://software-dl.ti.com/processor-sdk-rtos/esd/docs/04_03_00_05/rtos/DSP_Software.html#dsp-optimized-libraries
Can you confirm that the different lib for C674x like DSP lib, math lib, ..etc are not included in the processor SDK?
What is the way to proceed to use the different libs (DSP, math) within the processor SDK?
2) McBSP does not seem to be listed in the peripherals supported for OMAP-L13x/C674x.
Any plan to add McBSP support?
Do we have any McBSP example outside of the processor SDK?
Is there for example an example as part of the Diagnostic SW (for OMAP-L137 EVM)? or part of the CSL SW?
The former Starterware does not have support for McBSP.
3) The below demos seems to only be supported on OMAP-L137 EVM.
Any plan to have it on the C6748/OMAP-L138 LCDK?
http://software-dl.ti.com/processor-sdk-rtos/esd/docs/04_03_00_05/rtos/Examples_and_Demonstrations.html#audio-benchmark-starterkit
http://software-dl.ti.com/processor-sdk-rtos/esd/docs/04_03_00_05/rtos/Examples_and_Demonstrations.html#audio-pre-processing-demohttp://software-dl.ti.com/processor-sdk-rtos/esd/docs/04_03_00_05/rtos/Examples_and_Demonstrations.html#image-processing-demo
Thanks in advance,
Anthony