Part Number: RFSDK
Other Parts Discussed in Thread: TCI6630K2L, ADC12J4000, 66AK2L06
Hello
I am using an ADC12J4000 EVM connected to the 66AK2L06 EVM via JESD204B interface directly.
There are no additional things connected to 66AK2L06 EVM.
I don't know that what error's reason
Traceback (most recent call last):
File "/usr/bin/radio", line 115, in <module>
command.cmdloop()
File "/usr/lib/python2.7/cmd.py", line 142, in cmdloop
stop = self.onecmd(line)
File "/usr/lib/python2.7/cmd.py", line 221, in onecmd
return func(arg)
File "/usr/lib/python2.7/rfsdk/command.py", line 1023, in do_reset
self.radio.radio_reset()
File "/usr/lib/python2.7/rfsdk/radio.py", line 1127, in radio_reset
self.dfe.dfe_reset()
File "/usr/lib/python2.7/rfsdk/platform/TCI6630K2L.py", line 428, in dfe_reset
res = self.dfeS.CppDmaStatus()
File "/usr/lib/python2.7/dfe/service.py", line 502, in CppDmaStatus
rsp = self.run(rfsdk.RFSDK_API_MSGQ_SQCR2DFE, msg, res.sizeof()/4+2)
File "/usr/lib/python2.7/rfsdk/base.py", line 151, in run
raise rfsdk.Error("Problem contacting the RFSDK service at %s:%d" % (self.address, self.port))
rfsdk.Error: Problem contacting the RFSDK service at 127.0.0.1:50001
Please tell me what can I do to fix the error?
Seunggu Jeong