Part Number: TMS320C6670
Tool/software: Code Composer Studio
Hello.
I'm using starter kit tmdsevm6670l.
On the board there are two flashes. Over the PCI-interface there is SPI Flash "NOR128M-bit N25Q128A21BSF40F" on my board tmdsevm6670l.
Over the GPIO-interface there is NAND Flash "NAND512R3A2DZA6E" on my board tmdsevm6670l.
I want to burn one of two flashes with my program for 6670. My program should be loaded from the flash into 6670 after power is turned on.
Please tell me how can I burn ma flashes? May be you can adwice any example program to burn my out-file into my psi-flash or gpio-flash?
It would be greatful for me to now how can I do it.
Thanks a lot.
Ilya