Tool/software: Linux
Hello Everyone,
We have developed our custom board which is mostly same as the AM571x idk.
Now we are facing some issue related to the PMIC. 
As per below circuit we are driving the 12 Volt using one gpio.
Now we have connect load on 12V_D1 then we are doing gpio6_8 high pin high then it work fine.
same case we have connect load on 12V_D2 then we are doing gpio6_8 high pin high then it work fine.
but if we connect load on both 12V_D1 and 12V_D2 and then after we doing gpio6_8 high then board will reboot again. as per our more research we found that PMIC REGEN1 (F8) pin is reseting during this.
so can anyone have idea why this thing happen?
is there any PMIC configuration need to be chnage for this?
Thanks & Best Regards,
Nikunj Patel