Other Parts Discussed in Thread: AM5718, DP83848-EP
Hi,
I will be using AM5718. It has a GbE switch subsystem. I will be porting Linux OS into AM5718.
My requirement is to have two 10/100 ethernet ports for AM5718... PHYs to be used is DP83848-EP....
1. one ethernet port will be standard ethernet port
2. Other one would be used for onboard MAC-to- MAC communication....
i will not be utilizing the switch functionality.
Can I configure Ethernet Subsystem as two separate emacs??
Does Linux allow such a configuration??
Can I have separate MAC IDs for both?? MAC to MAC communication needs to have a fixed MAC id
pls advice