I want to decode the CIF video stream which is encoded in H.264 on DM365 platform.
But The video is displayed not the whole screen(720X576) only a part of screen(352 X288) in the center.
How could I make the output of decode be full of the screen?
Resier?
But the resizer is work in continuous mode. The resizer API is not support in this mode?
Or other ways?
I use the decode demo in dvsdk_2_10_01_18.