This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320VC33: Update my DSP

Part Number: TMS320VC33
Other Parts Discussed in Thread: TMS320C6727B, TMS320C6455, TMS320C6457

I’m looking to update the DSP I use in a couple of products. I’m currently using the TMS320VC33-150.
Don’t mind if the cost is $100 per devices.

Devices I’ve seen on the TI web site:
TMS320C6727B
TMS320C6455
TMS320C6457

Things I Need:
1-External Interrupt to drive DSP software loop.
32-bit Interface databus (EMIF) for moving data to a CPU, FPGA, NOR Flash & SRAM.
3.3 V I/O interface.
64-bit double-precision floating-point arithmetic.
Run C code on bare metal.
At least double the processing power.

If anybody has a suggestion that would be appreciated.

Alan