Hi,
I'm student and i actually work on an audio app with the ezDSP5535 board. I want to transmit data since my phone (app developped with MIT App Inventor) and my board via BT connexion (HC-06 module). I used for that the UART_RX and UART_TX pin from the extension board P2. I can establish a connexion, but i read understanding values. I tried the functions UART_read and UART_fgetc from CSL lib to recover my data from my phone, but i only received char like "ø", "þ", ... And when i used i slider item on my app, who normally can pass 10 values, i just read one or two of these characters... I set the baud rate at 9600 for my BT module, and the input clock to 100000000 Hz.
I just want to read from my app a simple integer on one byte with your CSL library for UART, how i can proceed?
Thank you for your help.
Best regards.
Alex