Other Parts Discussed in Thread: LM10011, TPS53681, UCD9222, UCD9222-EP, TPS54424, TPS54521, TPS65400
Hi!
I have a new design with C6654 and I saw the evaluation board uses C6657 and UCD9222 but UCD9222 is NRND and the recommended replacement TPS53681 it looks like works with LM10011. I would like to design a power supply for this DSP.
Input voltage 12V, output CVDD 0.85-1.1V, output 3A (The excel calculator came to 2A)
It looks like I can take two solutions:
LM10011 with a DC-DC
Will this work as I see a design for 5A - http://www.ti.com/lit/df/tidr731/tidr731.pdf
and it not suggest me an alternative reference schematic for powering C6654 DSP
Second solution
I can use the solution from the eval board and can I replace UCD9222 with UCD9222-EP? Or how else can I do it? I would take the easier approach non-analog because I understand I have to program UCD9222-EP part the very first time?
Otherwise
Give me the most optimal solution. This is not a complex part and the current draw is only 3A max worst case. The excel calculator came to 2A.
Thanks,
Divakar