Hello,
I'm unable to find the SMV320C6727-SP JTAG timing parameters in the datasheet or any of the related literature, such as TMS/TDI setup and hold and min/max TDO delay from TCK. Where is this information?
Many thanks,
Will S.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm unable to find the SMV320C6727-SP JTAG timing parameters in the datasheet or any of the related literature, such as TMS/TDI setup and hold and min/max TDO delay from TCK. Where is this information?
Many thanks,
Will S.
Will,
I was very fortunate, and was able to locate source data for the timing.
Parameter MIN MAX UNIT
tc(TCK) Cycle time, TCK 35 - ns
tsu(TDIV-TCKH) Setup time, TDI/TMS valid before TCK high 10 - ns
th(TCKH-TDIV) Hold time, TDI/TMS valid after TCK high 7 - ns
tw(TRSTL) Pulse duration, TRSTn low 100 - ns
td(TCKL-TDOV) Delay time, TCK low to TDO valid 0 15 ns
If this answers your question, please click "Verify it as the answer"
Regards,
Wade