Other Parts Discussed in Thread: AM3358
Tool/software: Linux
Hi,
I am facing problem while booting Linux SDK on custom board having AM3358 as core part. The image stored into SD card and try boot from there.But its showing NO partition found as shown in below.
I have created the image by the following the process as shown official site for Linux SDK. A normal Debian Linux booting successfully but SDK Linux is not working.
so help me out.
Thanks in Advance.
This is debugging logs from my board.
===============================================================================================================================
U-Boot SPL 2018.01-g9d984f4548 (Apr 06 2019 - 07:42:30)
Trying to boot from MMC1
*** Warning - bad CRC, using default environment
U-Boot 2018.01-g9d984f4548 (Apr 06 2019 - 07:42:30 +0000)
CPU : AM335X-GP rev 2.1
Model: TI AM335x BeagleBone Black
DRAM: 512 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
** Bad device mmc 0 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: Could not get PHY for cpsw: addr 0
cpsw, usb_ether
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1(part 0) is current device
** No partition table - mmc 1 **
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
** No partition table - mmc 1 **
## Error: "bootcmd_nand0" not defined
starting USB...
USB0: Port not available.
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 98:84:e3:93:60:d6
HOST MAC de:ad:be:ef:00:00
RNDIS ready
missing environment variable: pxeuuid
Retrieving file: pxelinux.cfg/01-98-84-e3-93-60-d6
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 98:84:e3:93:60:d6
HOST MAC de:ad:be:ef:00:00
=============================================================================================================