Hi,
When using Extended Wait Mode; what are the restrictions on the W_SETUP, W_STROBE and W_HOLD CEnCFG-fields?
When reading the "AM17x/AM18x ARM Microprocessor External Memory Interface A (EMIFA)" (SPRUFV0A) document all I can find regarding restrictions is this:
"If Extended Wait Mode is enabled by setting the EW field in the asynchronous n configuration register (CEnCFG), these fields must be set to a value greater than zero." (see page 27).
However, the ."Technial Reference Manual" (SPRUH93D) specifies the followig:
"... a restriction is placed on the strobe period timing parameters when operating in Extended Wait mode. Specifically, the sum of the W_SETUP and W_STROBE fields must be greater than 4, ..." (see page 742).
Which one is it? If the latter one applies, are there any ways around those pretty slow time specs?
At the moment I'm running with W_SETUP=0, W_STROBE=1, W_HOLD=1 and it seems to work just fine.
Thanks!