Hello,
Can you please provide the junction-to-board thermal resistance of SM320C40GFS60? Only RΘJC and RΘJA are in the datasheet.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can you please provide the junction-to-board thermal resistance of SM320C40GFS60? Only RΘJC and RΘJA are in the datasheet.
Thanks!
Elisha,
This is still in queue to be modeled. Tentative completion is 6/18.
Regards,
Wade
Hello Wade,
I hope you are fine.
I was just wondering if the model file will still be released on June 18. Can you please update us?
Thank you!
Yes, that is the plan.
I do know the engineer that creates it has been out of the office, but I still expect it to be delivered soon.
Regards,
Wade
Hello Wade,
Will the model file still be released tonight? If it isn't, can you please update us when it can be released?
Thanks a lot and regards.
Unfortunately, there were a couple events that caused the queue to get delayed.
Current estimate for completion is end of this week.
Regards,
Wade
Thanks, Wade. I do hope it gets released soon.
Regards to you and the modeling team.
He accellerated the modelling due to missing the window.
Here are the results.
Theta JA-High K: 13.2
Theta JC, top : 0.6
Theta JB : 8.0
Psi JT : 0.1
Psi JB : 7.3
Theta JC,bottom: n/a
If this answers your question, please click "This Resolved My Issue"
Regards,
Wade
thermal