Other Parts Discussed in Thread: TIDA-01414, PCM9211
Dear Sir/Ms.
Customers refer to our TIDA-01414 Reference design.
However, the customer's product specifications are as follows
1. Only 3 speakers, 100W, 93dB
2. Input HDMI In (eARC function) *1, SPDIF *1 (OPT + COAX)
3. Output HDMI Out *1 to TV
3. Need to support ATMOS
Because the datsheet specification on the 66aK2G webpage is not complete, I would like to ask the following question, TIDA-01414 Reference design question
1. Does the 66aK2G support HDMI IN? and has an eACR function?
2. Does 66aK2G support SPDIF?
3. Dose 66aK2G support HDMI output to TV?
If you do not have the eACR support function, can 66aK2G connect the PCM9211, and support function what requested by the customer?
If the 66AK2G does not have the functionality required by the customer, can you suggest external parts?
Best Regards,
Kami Huang